EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches

Overview

Discrete I/O Profile example configuration functions

Functions

bool DIO_DEVICE_CFG_init (EI_API_ADP_T *pAdapter)
 Makes full initialization of factory reset values.
 
void DIO_DEVICE_CFG_apply (EI_API_ADP_T *pAdapter)
 Applies the discrete io device profile configuration data on stack.
 
bool DIO_DEVICE_CFG_callback (EI_API_CIP_NODE_T *pCipNode, uint16_t classId, uint16_t instanceId, uint16_t attrId, EI_API_CIP_ESc_t serviceCode, int16_t serviceFlag)
 Configuration callback to synchronize discrete io device profile non-volatile values with actual stack attribute values. Sets the new non-volatile data, if necessary.
 
void DIO_DEVICE_CFG_setDefaultWithoutComm (void)
 Sets discrete IO device profile factory default values to the profile part of non volatile runtime structure.
 
void DIO_DEVICE_CFG_setHeader (DEVICE_PROFILE_CFG_Header_t *pHeader)
 Sets header for non volatile runtime structure.
 
bool DIO_DEVICE_CFG_isValid (void)
 Checks header of non volatile runtime structure against discrete IO device profile header.
 
void * DIO_DEVICE_CFG_getRuntimeData (void)
 Provides pointer to runtime configuration non volatile data.
 
void * DIO_DEVICE_CFG_getFactoryResetData (void)
 Provides pointer to factory reset non volatile data.
 
uint32_t DIO_DEVICE_CFG_getLength (void)
 Provides size of runtime configuration or factory reset data.
 
static uint32_t DIO_DEVICE_CFG_applyIdentity (EI_API_ADP_T *pAdapter)
 Applies the identity object attributes on the stack.
 
static uint32_t DIO_DEVICE_CFG_applyTimeSync (EI_API_ADP_T *pAdapter)
 Applies the Time Sync object attributes on the stack.