EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
Datasheet

Supported EtherNet/IP™ Functionality

Feature Description Implementation
EtherNet/IP Device Class Adapter Yes
Scanner No
Device Profile Examples Generic Device (0x2B)
General Purpose Discrete I/O Device (0x07)
Yes
Device Configuration EDS File Yes
Connection Types Exclusive Owner Yes
Input Only Yes
Listen Only Yes
Connection Trigger Types Cyclic Yes
Application Triggered No
Change of State Yes
Maximum Connections Class 1 8
Class 3 32
Explicit Messaging Connected Yes
Unconnected Yes
Standard Objects Identity Object (0x01) Yes
Message Router Object (0x02) Yes
Assembly Object (0x04) Yes
Connection Manager Object (0x06) Yes
Time Sync Object (0x43) Yes
Device Level Ring Object (0x47) Yes
QoS Object (0x48) Yes
TCP/IP Interface Object (0xF5) Yes
Ethernet Link Object (0xF6) Yes
LLDP Management Object (0x109) Yes
LLDP Data Table Object (0x10A) Yes
Supported Elementary Data Types BOOL Yes
SINT Yes
INT Yes
DINT Yes
LINT Yes
USINT Yes
UINT Yes
UDINT Yes
ULINT Yes
REAL Yes
LREAL Yes
STRING Planned
BYTE Yes
WORD Yes
DWORD Yes
LWORD Yes
STRING2 Planned
SHORT_STRING Yes
EPATH Yes
Supported Constructed Data Types Formal Array Yes
IP Addressing Modes DHCP Yes
BOOTP Yes
Static Yes
VLAN tagging IEEE802.1Q, 3 bit PCP (8 levels) Yes
Switch queues 4
Statistics Media counters supported per interface (dual port switch) Yes
Interface counters supported per interface Yes
CIP Sync (PTP/IEEE1588) Supports Drives Profile : E2E clock Yes
PTP over UDP Yes
Transparent Clock supported Yes
Ordinary Clock supported Yes
Single and Two Step Clock supported Yes
Supported Network Features Link Layer Discovery Protocol (LLDP) Yes
Device Level Ring (DLR) Yes
Address Conflict Detection (ACD) Yes
Quality of Service (QoS) Yes
CIP Reset Services Identity Object Reset Services of Typ 0, 1, and 2
Device Level Ring (DLR) Beacon based Yes
Self configuring Yes
Min. beacon interval 200 µs
Min. beacon timeout 400 µs
Baud Rate 100 Mbit/s Yes
10 Mbit/s Yes
Duplex Mode Half Yes
Full Yes
Auto Negotiation Yes
Conformance ODVA CT21

Key Performance Parameters

Feature Description Setting
Process Data Image max. I/O assembly (size) 1480 Bytes
Connection Trigger Types and Cycle Times Cyclic (Class 1) 1 ms
Change of State 1 ms
Bridge Delay Min Bridge Delay 2.71 μs
Max Bridge Delay 3.19 μs

General Stack Parameters

The table below lists resource requirement for the Generic Device (0x2B) and Discrete I/O Device (0x07) examples. Please note that this application has only a limited functional scope that does not contain the basic web server that is include with the example code. More complex application code will result in higher ROM and RAM requirements.

Stack Memory Usage (LP-AM263P)
Generic Device Discrete I/O
Code 255.69 kB 263.1 kB
RO Data 67.47 kB 69.04 kB
RW Data 563.03 kB 563.17 kB

EtherNet/IP QuickConnect™

Scope

QuickConnect is an optional functionality that may be enabled on a node-by-node basis. When enabled, QuickConnect will allow EtherNet/IP devices to quickly power up and join an EtherNet/IP network.

QuickConnect connection time is comprised of several key time phases. One factor of the QuickConnect connection time is the devices power-up time. Another factor is the amount of time it takes a controller to detect the newly attached device and send a Forward Open request to start the connection process.

QuickConnect targets 500 ms as the time between initial power-up and the establisment of IO connections.

EtherNet/IP QuickConnect Target

QuickConnect measurements have been performed on the Texas Instruments LP-AM243 LaunchPad™ development kit and the TMDS64EVM AM64x evaluation module with an attached TMDS64DC01EVM AM64x IO-link and high-speed breakout card.

For the measurements an oscilloscope is connected to a GPIO pin on the particular board which was set to high on application start and reset to low on the first Forward Open request. The measurements were triggered by the MCU_PORz signals available on the evaluation modules. The power-up time is the time interval between the MCU_PORz signal and application start. The connection establishment is the time interval between application start and the detection of the Forward Open request.

Evaluation Module MCU_PORz Signal GPIO Pin
LP-AM243 Header J6 pin 56 GPIO1_21 Header J7 pin 57
TMDS64EVM Safety connector pin 24 GPIO0_41 TMDS64DC01EVM, header J8 pin 24

To enable GPIO control the example application shipped with the EtherNet/IP Adapter software is extended by two functions:

uint32_t gpioBaseAddr;
void GPIO_init(void)
{
gpioBaseAddr = (uint32_t) AddrTranslateP_getLocalAddr(CONFIG_GPIO0_BASE_ADDR);
GPIO_setDirMode(gpioBaseAddr, CONFIG_GPIO0_PIN, CONFIG_GPIO0_DIR);
}
void GPIO_set(bool set)
{
if(set)
GPIO_pinWriteHigh(gpioBaseAddr, CONFIG_GPIO0_PIN);
else
GPIO_pinWriteLow(gpioBaseAddr, CONFIG_GPIO0_PIN);
}

GPIO_init and GPIO_set are called in App.c at application start and later in the Forward Open callback function.

void EI_APP_mainTask(
void* pvTaskArg_p)
{
uint32_t err;
Board_init();
Drivers_open();
Board_driversOpen();
GPIO_init();
GPIO_set(true);
......

EtherNet/IP QuickConnect Controller

The QuickConnect controller device is emulated by a Python script that triggers the connection establishment upon detection of ARP announce frames.

ARP announce frame received Request of TCP connection Request of Register Session Forward Open request
0.0 ms 2.494 ms 15.215 ms 26.398 ms

EtherNet/IP QuickConnect Measurement Results

Evaluation Module Application start Forward Open Request
LP-AM243 252 ms 318 ms
TMDS64EVM 180 ms 269 ms