EtherNet/IP™ Adapter3.09.00
 
Loading...
Searching...
No Matches
Data Structures
Here are the data structures with brief descriptions:
 CAPP_DRIVERS_SInitApplication drivers initialization parameters
 CAPP_SAcd
 CAPP_SAdapter
 CAPP_SApplication
 CAPP_SHwal
 CAPP_SInstance
 CAPP_SLwip
 CAPP_SParams
 CCMN_CPU_API_SData
 CCMN_CPU_API_SLoad
 CCMN_CPU_API_SParams
 CCUST_DRIVERS_SInitDrivers initialization parameters
 CCUST_EEPROM_SInit
 CCUST_ETHPHY_SInit
 CCUST_ETHPHY_SParams
 CCUST_FLASH_SInit
 CCUST_LED_SInit
 CDEVICE_PROFILE_CFG_AdapterData
 CDEVICE_PROFILE_CFG_Data
 CDEVICE_PROFILE_CFG_Header
 CDEVICE_PROFILE_CFG_ProfileData
 CDEVICE_PROFILE_CFG_SInitInitialization parameters of non-volatile configuration data
 CDEVICE_PROFILE_INTF_Interface
 CDEVICE_PROFILE_NVM_SInitNon-Volatile memory initialization parameters
 CDEVICE_PROFILE_NVM_SWriteParamNon-Volatile memory write parameters
 CDIO_DEVICE_ASM_container
 CDIO_DEVICE_CFG_DataDeclaration of whole non volatile data structure
 CDIO_DEVICE_CFG_ProfileDataDeclaration of non volatile data structure related to discrete IO device profile
 CDIO_DEVICE_DIP_ClassDataA structure to hold Discrete Input Point's (DIP) class data
 CDIO_DEVICE_DIP_container
 CDIO_DEVICE_DIP_object
 CDIO_DEVICE_DIP_ObjectCfgDIP Object configuration structure
 CDIO_DEVICE_DOG_ClassDataA structure to hold Discrete Output Group's (DOG) class data
 CDIO_DEVICE_DOG_container
 CDIO_DEVICE_DOG_object
 CDIO_DEVICE_DOG_ObjectCfgDOG Object Configuration structure
 CDIO_DEVICE_DOP_ClassDataA structure to hold Discrete Output Point's (DOP) class data
 CDIO_DEVICE_DOP_container
 CDIO_DEVICE_DOP_object
 CDIO_DEVICE_DOP_ObjectCfgDOP Object configuration structure
 CDIO_DEVICE_DOP_Value
 CDRIVERS_SInitDrivers initialization parameters
 CDRV_BOARD_INFO_SBlockHeaderStructure to store the block header
 CDRV_BOARD_INFO_SMacIdHeaderStructure to store the block MAC ID header
 CDRV_BOARD_INFO_SMainHeaderStructure to store the board info header
 CDRV_BOARD_SEeprom
 CDRV_BOARD_SInitApplication UART driver initialization parameters
 CDRV_BOARD_SMac
 CDRV_BOARD_SObject
 CDRV_COMMON_Mutex_container
 CDRV_EEPROM_SInit
 CDRV_FLASH_SInit
 CDRV_LED_Industrial
 CDRV_LED_SInitApplication LED's initialization parameters
 CDRV_PRUICSS_ConfigParams
 CDRV_PRUICSS_PRU_Config
 CDRV_PRUICSS_PRU_EthPhy
 CDRV_PRUICSS_PRU_Mdio
 CDRV_PRUICSS_SInit
 CDRV_Uart
 CDRV_UART_SInitApplication UART driver initialization parameters
 CEI_API_ADP_SCmgrForwardCloseInfo
 CEI_API_ADP_SCmgrForwardOpenInfoDefinition for ConnectionManager callback functions
 CEI_API_ADP_SCurrentIpData
 CEI_API_ADP_SEipStatus
 CEI_API_ADP_SInit
 CEI_API_ADP_SIntfConfBitsGeneral Interface attribute parameter collection
 CEI_API_ADP_SLldp_ParameterNonvolatile attribute parameter of LLDP Management object
 CEI_API_ADP_SMcastConfigGeneral multi-cast attribute parameter collection
 CEI_API_ADP_SModNetStatusGeneral adapter status collection
 CEI_API_ADP_SParam
 CEI_API_ADP_SPortState
 CEI_API_ADP_SQosGeneral QoS attribute parameter collection
 CEI_API_ADP_SRevision
 CEI_API_ADP_UCmgrInfo
 CEI_API_ADP_UIntfConfStructure to use as function parameter (attribute parameters)
 CEI_API_CIP_NODE_InitParamsInitialization parameters to create new CIP Node
 CEI_API_CIP_SAssemCustomMapCustom Assembly mapping structure
 CEI_API_CIP_SAssemMapDataData structure used during callback in custom-map assemblies
 CEI_API_CIP_SAttrGeneral attribute parameter collection
 CEI_API_CIP_SBufferConsumer/Producer buffer structure declaration
 CEI_API_CIP_SCustomServiceCustom service structure declaration
 CEI_API_CIP_SServiceGeneral service parameter collection
 CEI_API_CIP_STransferBuffer
 CEIP_SConfigurationControl_t
 CEIP_SLoadParameter
 CEIP_SPortState
 CGENERIC_DEVICE_CFG_DataDeclaration of whole non volatile data structure
 CGENERIC_DEVICE_CFG_ProfileDataDeclaration of non volatile data structure related to generic device profile
 CIcve_macAddr_s
 CIcve_message_s
 CIcve_msgHeader_s
 CIcve_notifyMsg_s
 CIcve_reqMsg_s
 CIcve_respMsg_s
 CIcve_ShrMemInfo_s
 CIcve_ShrMemQInfo_s
 Cinterim_report
 Cperf_stats
 CTaskP_Ctrl
 CTaskP_Struct_
 CtskTaskControlBlock
 CWEB_SERVER_SParams