#include <ecSlvApiInternal.h>
Data Fields | |
| EC_API_EError_t | status |
| error code if parsing failed | |
| bool | needInputMapping |
| if set the next cycle trigger pd update on pru | |
| uint32_t | watchdogInterval |
| watchdog monitor interval in ms | |
| uint32_t | watchdogState |
| current watchdog state | |
| uint8_t | lastAppstate |
| remember appstate | |
| uint8_t | rsvd [3] |
| alignment | |
| EC_API_EError_t | lastCyclicError |
| Last Cyclic error. | |
| bool | sscValidLicense |
| SSC License is valid. | |
| bool | beckhoffStarted |
| Stack runs in OP State. | |