EtherCAT SubDevice
 
Loading...
Searching...
No Matches
EC_SLV_INT_SDIAG_parameter Struct Reference

EC_API_SLV_SDIAG_parameter_t Diagnosis type parameter. More...

#include <ecSlvApi_types.h>

Data Fields

uint16_t defType
 paramter type (DEFTYPE_UNSIGNED8, DEFTYPE_UNSIGNED16...)
 
uint8_t msgType
 message type (DIAG_MSG_PARAM_TYPE_DATA, DIAG_MSG_PARAM_TYPE_B_ARRY...)
 
uint32_t length
 param length
 
uint8_t * pParam
 pointer to the corresponding parameter memory
 

Detailed Description

EC_API_SLV_SDIAG_parameter_t Diagnosis type parameter.