#include <ecSlvApiInternal.h>
Data Structures | |
| struct | EC_SLV_INT_GEN_MetaInfo |
Data Fields | |
| struct EC_SLV_INT_General::EC_SLV_INT_GEN_MetaInfo | metaInfo |
| uint16_t | eePDICtrl |
| PDI control value. | |
| uint16_t | eePDICfg |
| PDI configuration value. | |
| bool | eePDICtrlSet |
| PDI control set by user. | |
| bool | eePDICfgSet |
| PDI configuration set by user. | |
| EC_SLV_API_SSyncManDesc_t | bootStrapMbx [2] |
| Bootstrap mailbox configuration. | |
| bool | bootStrapMbxSet [2] |
| Bootstrap mailbox configuration set by user. | |
| EC_SLV_API_SSyncManDesc_t | standardMbx [2] |
| Standard mailbox configuration. | |
| bool | standardMbxSet [2] |
| Standard mailbox configuration set by user. | |
| EC_SLV_API_SSyncManDesc_t | syncManCfg [4] |
| SyncManager configuration. | |
| bool | syncManCfgSet [4] |
| SyncManager configuration set by user. | |
| uint16_t | stationAlias |
| Station Alias value. | |
| uint16_t | rsvd |
| alignment | |
| bool | fwInstallRequired |
| Firmware update triggered. | |
| uint32_t | maxPDOutputDataSize |
| Output process data size. | |
| uint32_t | maxPDInputDataSize |
| Input process data size. | |