EtherCAT SubDevice
 
Loading...
Searching...
No Matches
EC_API_SLV_SEeprom Struct Reference

#include <ecSlvInternal_eeprom.h>

Data Fields

uint16_t pdiControl
 
uint16_t pdiConfiguration
 
uint16_t syncImpulseLen
 
uint16_t pdiConfiguration2
 
uint16_t station_alias
 
uint16_t reserved0 [2]
 
uint16_t checksum
 
uint32_t vendorID
 
uint32_t productCode
 
uint32_t revisionNo
 
uint32_t serialNo
 
uint16_t executionDelay
 
uint16_t port0Delay
 
uint16_t port1Delay
 
uint16_t reserved1
 
uint16_t bootstrapReceiveMailboxOffset
 
uint16_t bootstrapReceiveMailboxSize
 
uint16_t bootstrapSendMailboxOffset
 
uint16_t bootstrapSendMailboxSize
 
uint16_t standardReceiveMailboxOffset
 
uint16_t standardReceiveMailboxSize
 
uint16_t standardSendMailboxOffset
 
uint16_t standardSendMailboxSize
 
uint16_t mailboxProtocol
 
uint16_t reserved2 [33]
 
uint16_t kBitSize
 
uint16_t version