#include <ecSlvApiInternal.h>
Data Fields | |
| EC_API_SLV_SCoE_ObjEntry_t * | pEntries |
| Pointer to the SDO Entries. | |
| uint16_t | entries |
| Number of entries. | |
| uint8_t | highestEntry |
| Record types may not contain consecutive subIndexes, thus store highest subIdx Entry. | |
| uint8_t | rsvd |
| alignment | |
| TOBJECT | sscLayerObject |
| SSC SDO Object. | |
| void * | cbReadCtxt |
| Read callback context. | |
| EC_API_SLV_CBObjRead_t | cbRead |
| Read callback. | |
| void * | cbWriteCtxt |
| Write callback context. | |
| EC_API_SLV_CBObjWrite_t | cbWrite |
| Write callback. | |
| struct EC_API_SLV_CoE_Object * | pNext |
| Next Object. | |