#include <ecSlvApiInternal.h>
Data Fields | |
| uint16_t | index |
| Object Index number. | |
| uint8_t | subIndex |
| Object SubIndex number. | |
| uint8_t | rsvd |
| alignment | |
| char * | pName |
| Object entry name. | |
| uint8_t * | pVarPtr |
| Pointer to data memory space. | |
| uint32_t | enumValue |
| Enum Value. | |
| void * | enumMemory |
| Enum Memory area. | |
| TSDOINFOENTRYDESC * | pSdoEntryInfo |
| Object entry descriptor. | |
| struct EC_API_SLV_CoE_ObjEntry * | pNext |
| Pointer to next entry. | |