Software installation
Connect the development board
LP-AM263PX
Board details: LP-AM263P
- Setup a dip switches on the board : OSPI Boot Mode
- This mode is used to boot flashed applications via EVM flash like OSPI flash.
OSPI Boot Mode
- Connect the evaluation board to your computer using a micro-USB cable:
- J34 JTAG interface (XDS110) and UART console
USB connector on the AM263px LP Board
- Connect an ethernet cable from a PC running the TwinCAT to EtherCAT IN/Port0 of the PRU-ICSS on the development board.
EtherCAT connectors on the AM263px LP Board
- If you have multiple devices in chain, please connect from EtherCAT OUT/Port1 to IN/Port0 of next device. For the last device in chain, OUT/Port1 will be left open (if NOT using redundancy mode).
- Connect a USB Type-C Power Supply to the board
Board power connector on the AM263px LP
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu , see Using SDK with CCS Projects
- When using makefiles to build, note the required combination and build using make command , see Using SDK with Makefiles