EtherCAT SubDevice
Loading...
Searching...
No Matches
Example
Take a look at the GPIO LED example on the page
GPIO LED example
When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu, see
\iline 22 Using SDK with CCS Projects
.
When using makefiles to build, note the required combination and build using make command, see
\iline 23 Using SDK with Makefiles
.
Launch a CCS debug session and run the executable, see
\iline 24 CCS Launch, Load and Run
.
generated by
1.9.8