EtherCAT SubDevice
 
Loading...
Searching...
No Matches
Known Issues
Id Summary Description
DTKEC-195 Enable bootstrap only if FoE is used If the application does not use FoE, then the SDK DTK must not show bootstrap information; otherwise, the device claims bootstrap supported but the ESI file does not. This is an error on the Conformance Test Protocol.