| uint32_t EC_API_SLV_cbRegisterStartMbxHandler | ( | EC_API_SLV_SHandle_t * | pHandle, |
| EC_API_SLV_CBStartMbxHandler_t | cbFunc, | ||
| void * | pContext | ||
| ) |
This is the function to register a function which starts the mailbox handler.
The function is called in the state transition from INIT to PREOP when all general settings were checked to start the mailbox handler. This function informs the application about the state transition, the application can refuse the state transition when returning an AL Status error code. The return code NOERROR_INWORK can be used, if the application cannot confirm the state transition immediately, in that case this function will be called cyclically until a value unequal NOERROR_INWORK is returned
| [in] | pHandle | The pointer to the EtherCAT API instance. |
| [in] | cbFunc | Function pointer to the Start Mailbox Handler |
| [in] | pContext | startMbxHandler call context |