EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_PDO_setData()

uint32_t EC_API_SLV_PDO_setData ( EC_API_SLV_SHandle_t pHandle,
EC_API_SLV_Pdo_t pPdo,
uint32_t  length,
uint8_t *  pData 
)

Write PDO content into Process Image. All PDO entries are written in a data chunk.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]pPdopointer to PDO instance
[in]lengthdata length in bytes
[in]pDatapointer to data
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
// the Call
retVal = EC_API_SLV_PDO_setData(ptEcSlvApi, ptRxPdo, length, data);
uint32_t EC_API_SLV_PDO_setData(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_Pdo_t *pPdo, uint32_t length, uint8_t *pData)
Write PDO content into Process Image. All PDO entries are written in a data chunk.
Definition ecSlvApi_pdo.c:1142