EtherCAT SubDevice
Loading...
Searching...
No Matches
◆
EC_API_SLV_PDO_getEntryCount()
uint32_t EC_API_SLV_PDO_getEntryCount
(
EC_API_SLV_SHandle_t
*
pHandle
,
EC_API_SLV_Pdo_t
*
pPdo
,
uint8_t *
pCount
)
Read PDO entry count.
Parameters
[in]
pHandle
The pointer to the EtherCAT API instance.
[in]
pPdo
PDO instance.
[out]
pCount
Number of entries.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
uint8_t count =
EC_API_SLV_PDO_getEntryCount
(ptPdo);
EC_API_SLV_PDO_getEntryCount
uint32_t EC_API_SLV_PDO_getEntryCount(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_Pdo_t *pPdo, uint8_t *pCount)
Read PDO entry count.
Definition
ecSlvApi_pdo.c:2008
See also
EC_API_SLV_PDO_getEntryDataLength
PDO Configuration
generated by
1.9.8