| uint32_t EC_API_SLV_PDO_getEntryData | ( | EC_API_SLV_SHandle_t * | pHandle, |
| EC_API_SLV_Pdo_t * | pPdo, | ||
| uint8_t | subIndex, | ||
| uint32_t | length, | ||
| uint8_t * | pData | ||
| ) |
Read data from an individual PDO Entry Variable.
| [in] | pHandle | The pointer to the EtherCAT API instance. |
| [in] | pPdo | pointer to PDO instance |
| [in] | subIndex | PDO entry number |
| [in] | length | data length in bytes |
| [in] | pData | pointer to data |