EtherCAT SubDevice
Loading...
Searching...
No Matches
◆
EC_API_SLV_getInputProcDataLength()
uint32_t EC_API_SLV_getInputProcDataLength
(
EC_API_SLV_SHandle_t
*
pHandle
,
uint32_t *
pLength
)
Read the input process data length.
Parameters
[in]
pHandle
The pointer to the EtherCAT API instance.
[out]
pLength
input process data length in bits.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
uint32_t length =
EC_API_SLV_getInputProcDataLength
(ptEcSlvApi);
EC_API_SLV_getInputProcDataLength
uint32_t EC_API_SLV_getInputProcDataLength(EC_API_SLV_SHandle_t *pHandle, uint32_t *pLength)
Read the input process data length.
Definition
ecSlvApi_pdo.c:1925
See also
EC_API_SLV_getOutputProcDataLength
Examples
ESL_cia402Demo.c
.
PDO Configuration
generated by
1.9.8