| uint32_t EC_API_SLV_cbRegisterSystemReboot | ( | EC_API_SLV_SHandle_t * | pHandle, |
| EC_API_SLV_CBSystemRebootHandler_t | cbFunc, | ||
| void * | pContext | ||
| ) |
This is the function to register the Reboot function.
This function registers a function pointer which must be implemented by the user. The user defined function will be called after the firmware is correctly updated
| [in] | pHandle | The pointer to the EtherCAT API instance. |
| [in] | cbFunc | Function pointer to the Reboot function |
| [in] | pContext | systemReboot call context |