EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_EoE_cbRegisterSettingIndHandler()

uint32_t EC_API_SLV_EoE_cbRegisterSettingIndHandler ( EC_API_SLV_SHandle_t pHandle,
EC_API_SLV_EoE_CBSettingIndHandler_t  cbFunc,
void *  pContext 
)

This is the function to register EoE Setting Indication handler.

This function registers a function pointer which must be implemented by the user. The user defined function will be called any time an EoE Setting Indication is received.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]cbFuncFunction pointer to the EoE Setting Indication Handler
[in]pContextEoE settingIndHandler call context
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_EoE_cbRegisterSettingIndHandler(ecSlaveApi, cbFunc, pCtxt);
uint32_t EC_API_SLV_EoE_cbRegisterSettingIndHandler(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_EoE_CBSettingIndHandler_t cbFunc, void *pContext)
This is the function to register EoE Setting Indication handler.
Definition ecSlvApi_EoE.c:89