EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_EEPROM_cbRegisterInit()

uint32_t EC_API_SLV_EEPROM_cbRegisterInit ( EC_API_SLV_SHandle_t pHandle,
EC_API_SLV_CBEepromInit_t  cbFunc,
void *  pContext 
)

Initialize flash memory block.

Parameters
[in]pHandleSlave API Handle Instance
[in]cbFuncInit flash block Callback
[in]pContextflashInit call context
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_CBInitFlash_t cbFunc;
// the Call
uint32_t EC_API_SLV_EEPROM_cbRegisterInit(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_CBEepromInit_t cbFunc, void *pContext)
Initialize flash memory block.
Definition ecSlvApi.c:2403
Definition ecSlvApiInternal.h:331
Examples
ecSubDeviceCiA402.c.