| uint32_t EC_API_SLV_DIAG_newMessage | ( | EC_API_SLV_SHandle_t * | pHandle, |
| uint32_t | diagCode, | ||
| uint8_t | type, | ||
| uint16_t | textID, | ||
| uint8_t | numParams, | ||
| EC_API_SLV_SDIAG_parameter_t * | pParams | ||
| ) |
Send Diagnosis message.
| [in] | pHandle | DTK API instance. |
| [in] | diagCode | Diagnosis code. |
| [in] | type | Diagnosis type. |
| [in] | textID | Diagnosis text ID. |
| [in] | numParams | Number of parameters. |
| [in] | pParams | Diagnosis parameters. |