| uint32_t EC_API_SLV_CoE_configEnum | ( | EC_API_SLV_SHandle_t * | pHandle, |
| EC_API_SLV_SCoE_Object_t * | object, | ||
| uint32_t | value, | ||
| char * | name | ||
| ) |
This function creates an ENUN Object.
| [in] | ecSlaveApi | The pointer to the EtherCAT API instance. |
| [in] | object | pointer to SDO instance. |
| [in] | value | ENUM value. |
| [in] | name | ENUM name. |