EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_CoE_getObjectEntryCount()

uint32_t EC_API_SLV_CoE_getObjectEntryCount ( EC_API_SLV_SHandle_t pHandle,
EC_API_SLV_SCoE_Object_t pObject,
uint8_t *  pCount 
)

This function returns the number of entries of an Object.

Returns the number of entries of an Object

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]pObjectpointer to the object instance
[out]pCountnumber of entries of the object
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint8_t count = 0;
i32uErr_l = EC_API_SLV_CoE_getObjectEntryCount(ecSlaveApi, ptObject, &count);
uint32_t EC_API_SLV_CoE_getObjectEntryCount(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_SCoE_Object_t *pObject, uint8_t *pCount)
This function returns the number of entries of an Object.
Definition ecSlvApi_CoE.c:492
See also
EC_API_SLV_CoE_getObject EC_API_SLV_CoE_getObjectData EC_API_SLV_CoE_setObjectEntryData