EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_CoE_getObject()

uint32_t EC_API_SLV_CoE_getObject ( EC_API_SLV_SHandle_t pHandle,
uint16_t  index,
EC_API_SLV_SCoE_Object_t **  ppObject 
)

This function returns an object of the Object Dictionary.

Get Object of Object Dictionary

Parameters
[in]pHandleThe instance.
[in]indexObject index
[out]ppObjectObject object
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
uint32_t retVal = 0;
EC_API_SLV_SCoE_Object_t* ptObject= NULL;
// the Call
retVal = EC_API_SLV_CoE_getObject(S_ecSlvApiHdl, 0x2002, &ptObject);
uint32_t EC_API_SLV_CoE_getObject(EC_API_SLV_SHandle_t *pHandle, uint16_t index, EC_API_SLV_SCoE_Object_t **ppObject)
This function returns an object of the Object Dictionary.
Definition ecSlvApi_CoE.c:285
Definition ecSlvApiInternal.h:143
Definition ecSlvApiInternal.h:331
See also
EC_API_SLV_CoE_getObjectEntry EC_API_SLV_setObjectData EC_API_SLV_CoE_getObjectEntryData
Examples
ESL_cia402Demo.c.