#include <ecSlvApi.h>
uint32_t EC_API_SLV_CoE_configRecordSubIndex(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_SCoE_Object_t *pObject, uint8_t subIndex, char *pName, uint16_t type, uint16_t bitLen, uint16_t flags)
This function creates a subIndex for the Record Object.
Definition ecSlvApi_CoE.c:3268
uint32_t EC_API_SLV_CoE_odAddRecord(EC_API_SLV_SHandle_t *pHandle, uint16_t index, char *pName, EC_API_SLV_CBObjRead_t cbRead, void *pReadCtxt, EC_API_SLV_CBObjWrite_t cbWrite, void *pWriteCtxt, EC_API_SLV_SCoE_Object_t **ppOutSdo)
This function creates a Record Object.
Definition ecSlvApi_CoE.c:1974
#define ACCESS_READWRITE
Read/write in all states.
Definition ecSlvApiDef_CoE.h:134
#define ACCESS_READ
Read only in all states.
Definition ecSlvApiDef_CoE.h:135
#define OBJACCESS_TXPDOMAPPING
Mappable in TxPDOs.
Definition ecSlvApiDef_CoE.h:145
#define OBJACCESS_RXPDOMAPPING
Mappable in RxPDOs.
Definition ecSlvApiDef_CoE.h:144
#define DEFTYPE_INTEGER32
INTEGER32.
Definition ecSlvApiDef_CoE.h:43
Definition ecSlvApiInternal.h:143