EtherCAT SubDevice
Loading...
Searching...
No Matches
◆
EC_API_SLV_CiA402_activateAxis()
uint32_t EC_API_SLV_CiA402_activateAxis
(
EC_API_SLV_SHandle_t
*
pHandle
,
uint8_t
axisNo
,
bool
active
)
Activate Axis.
Parameters
[in]
pHandle
Slave API Handle Instance
[in]
axisNo
Number of Axis.
[in]
active
activate axis.
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t
* S_ecSlvApiHdl;
uint8_t axisNo;
bool
active;
// the Call
EC_API_SLV_CiA402_activateAxis
(S_ecSlvApiHdl, axisNo, active);
EC_API_SLV_CiA402_activateAxis
uint32_t EC_API_SLV_CiA402_activateAxis(EC_API_SLV_SHandle_t *pHandle, uint8_t axisNo, bool active)
Activate Axis.
Definition
ecSlvApi_CiA402.c:298
EC_API_SLV_Handle
Definition
ecSlvApiInternal.h:331
Examples
ESL_cia402Demo.c
.
CiA402 functions and callbacks
generated by
1.9.8