EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_CiA402_registerSetDictValues()

uint32_t EC_API_SLV_CiA402_registerSetDictValues ( EC_API_SLV_SHandle_t pHandle,
EC_API_SLV_CiA402_CBUsrApplSetDictValues_t  cbFunc,
void *  pContext 
)

Set values for configured CiA402 Object Dictionary objects.

Parameters
[in]pHandleSlave API Handle Instance
[in]cbFuncHandle to set CiA402 Device Specific Object Dictionary values.
[in]pContextCiA402 setDictValues call context
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_CiA402_registerSetDictValues(S_ecSlvApiHdl, cbFunc, pCtxt);
void(* EC_API_SLV_CiA402_CBUsrApplSetDictValues_t)(void *pContext)
Set default values for the CiA402 Objects.
Definition ecSlvApi_types.h:905
uint32_t EC_API_SLV_CiA402_registerSetDictValues(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_CiA402_CBUsrApplSetDictValues_t cbFunc, void *pContext)
Set values for configured CiA402 Object Dictionary objects.
Definition ecSlvApi_CiA402.c:89
Definition ecSlvApiInternal.h:331
Examples
ecSubDeviceCiA402.c.