| uint32_t EC_API_SLV_setVendorId | ( | EC_API_SLV_SHandle_t * | pHandle, |
| uint32_t | vendorId | ||
| ) |
Set device vendor ID. Used by the EEPROM and Object Dictionary.
Set a vendor ID. Required for device identification. It is used by the SII interface and the Object Dictionary
| [in] | pHandle | The pointer to the EtherCAT API instance. |
| [in] | vendorId | vendor identification number. |