EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_setGroupType()

uint32_t EC_API_SLV_setGroupType ( EC_API_SLV_SHandle_t pHandle,
char *  pGroupType 
)

Set device group name.

Set a group name for the device. Required by the Object Dictionary

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]pGroupTypegroup name.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_setGroupType(S_ecSlvApiHdl, "KUNBUS Fieldbus Development Toolkit");
uint32_t EC_API_SLV_setGroupType(EC_API_SLV_SHandle_t *pHandle, char *pGroupType)
Set device group name.
Definition ecSlvApi_param.c:335
Definition ecSlvApiInternal.h:331
See also
EC_API_SLV_setVendorId, EC_API_SLV_setProductCode, EC_API_SLV_setRevisionNumber, EC_API_SLV_getProductName
Examples
ecSubDeviceCiA402.c.