EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_setSerialNumber()

uint32_t EC_API_SLV_setSerialNumber ( EC_API_SLV_SHandle_t pHandle,
uint32_t  serialNumber 
)

Set default serial number.

Set a default serial number for the device. (ESC recommendation is to use boar HW serial)

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]serialNumberproduct serial number.
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_setSerialNumber(S_ecSlvApiHdl, 0x00000000);
uint32_t EC_API_SLV_setSerialNumber(EC_API_SLV_SHandle_t *pHandle, uint32_t serialNumber)
Set default serial number.
Definition ecSlvApi_param.c:224
Definition ecSlvApiInternal.h:331
See also
EC_API_SLV_getSerialNumber
Examples
ecSubDeviceCiA402.c.