EtherCAT SubDevice
Loading...
Searching...
No Matches
◆
EC_API_SLV_getSwVersion()
uint32_t EC_API_SLV_getSwVersion
(
EC_API_SLV_SHandle_t
*
pHandle
,
char **
ppSwVersion
)
Get serial number.
Get serial number. Used by the Object Dictionary
Parameters
[in]
pHandle
EtherCAT API instance.
[out]
ppSwVersion
Software version.
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
EC_API_SLV_SHandle_t
* S_ecSlvApiHdl;
char
* swVersion = NULL;
// the Call
swVersion =
EC_API_SLV_getSwVersion
(S_ecSlvApiHdl);
EC_API_SLV_getSwVersion
uint32_t EC_API_SLV_getSwVersion(EC_API_SLV_SHandle_t *pHandle, char **ppSwVersion)
Get serial number.
Definition
ecSlvApi_param.c:1172
EC_API_SLV_Handle
Definition
ecSlvApiInternal.h:331
See also
EC_API_SLV_setSwVersion
Parameter Configuration
generated by
1.9.8