EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_setSyncManErrLimit()

uint32_t EC_API_SLV_setSyncManErrLimit ( EC_API_SLV_SHandle_t pHandle,
uint16_t  smErrorLimit 
)

Set SyncManager sequence error counter limit.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]smErrorLimitSM sequence error counter limit
Returns
uint32_t Returns the API error code.
Example
#include <ecSlvApi.h>
// required variables
uint32_t retVal = 0;
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
// the Call
retVal = EC_API_SLV_setSyncManErrLimit(S_ecSlvApiHdl, 0xff);
uint32_t EC_API_SLV_setSyncManErrLimit(EC_API_SLV_SHandle_t *pHandle, uint16_t smErrorLimit)
Set SyncManager sequence error counter limit.
Definition ecSlvApi_param.c:816
Definition ecSlvApiInternal.h:331
Examples
ecSubDeviceCiA402.c.