| uint32_t EC_API_SLV_setRevisionNumber | ( | EC_API_SLV_SHandle_t * | pHandle, |
| uint32_t | revisionNumber | ||
| ) |
Set device revision number. Used by the EEPROM and Object Dictionary.
Set a product code. Required for device identification. It is used by the SII interface and the Object Dictionary
| [in] | pHandle | The pointer to the EtherCAT API instance. |
| [in] | revisionNumber | product revision number. |