EtherCAT SubDevice
Loading...
Searching...
No Matches
◆
EC_API_SLV_postSeqInputPDBuffer()
uint32_t EC_API_SLV_postSeqInputPDBuffer
(
EC_API_SLV_SHandle_t
*
pHandle
,
uint32_t
length
,
void *
pData
)
Release Tx Buffer.
Parameters
[in]
pHandle
pointer to API instance.
[in]
pData
Send allocated buffer.
[in]
length
length of buffer
Returns
error code
Example
#include <ecSlvApi.h>
// required variables
EC_API_SLV_SHandle_t
* pHandle;
void
* pvBuffer;
// the Call
retVal =
EC_API_SLV_postSeqInputPDBuffer
(pHandle, pvBuffer);
EC_API_SLV_postSeqInputPDBuffer
uint32_t EC_API_SLV_postSeqInputPDBuffer(EC_API_SLV_SHandle_t *pHandle, uint32_t length, void *pData)
Release Tx Buffer.
Definition
ecSlvApi_pdo.c:2578
EC_API_SLV_Handle
Definition
ecSlvApiInternal.h:331
See also
EC_API_SLV_preSeqInputPDBuffer
Examples
ESL_cia402Demo.c
.
Buffer Handling API
generated by
1.9.8