EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_cbRegisterBoardStatusLed()

uint32_t EC_API_SLV_cbRegisterBoardStatusLed ( EC_API_SLV_SHandle_t pHandle,
EC_API_SLV_CBBoardStatusLed_t  cbFunc,
void *  pContext 
)

Register Board Status LED callback.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]pContexTboardStatusLED call context
[in]cbFuncFunction pointer to the FoE Open file Handler
[in]pLedContextLED context
Returns
ErrorCode API Error Code
Example
#include <theHeader.h>
// required variables
uint32_t retVal = 0;
void* pvVariable = NULL;
// the Call
retVal = EC_API_SLV_cbRegisterBoardStatusLed(ecSlaveApi, cbFunc, ctxt);
uint32_t EC_API_SLV_cbRegisterBoardStatusLed(EC_API_SLV_SHandle_t *pHandle, EC_API_SLV_CBBoardStatusLed_t cbFunc, void *pContext)
Register Board Status LED callback.
Definition ecSlvApi_board.c:102
Examples
ecSubDeviceCiA402.c.