EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_reset()

uint32_t EC_API_SLV_reset ( EC_API_SLV_SHandle_t pHandle)

Reset configuration to default values.

Reset Pdo Assignments, mappings and any configuration to default values

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
Returns
EC_API_EError_t Returns the API error code.
Example
#include <ecSlvApi.h>
EC_API_SLV_SHandle_t* S_ecSlvApiHdl;
uint32t retVal = 0;
// the Call
retVal = EC_API_SLV_reset(S_ecSlvApiHdl);
uint32_t EC_API_SLV_reset(EC_API_SLV_SHandle_t *pHandle)
Reset configuration to default values.
Definition ecSlvApi.c:1549
Definition ecSlvApiInternal.h:331