EtherCAT SubDevice
Loading...
Searching...
No Matches
◆
EC_API_SLV_writeDoubleWordEscRegister()
uint32_t EC_API_SLV_writeDoubleWordEscRegister
(
EC_API_SLV_SHandle_t
*
pHandle
,
uint16_t
escAddress
,
uint32_t
value
)
Write to ESC register.
Parameters
[in]
pHandle
The pointer to the EtherCAT API instance.
[in]
escAddress
The ESC Address
[in]
value
New value
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
uint32_t alEscCtrlStatus = 8;
// the Call
EC_API_SLV_writeByteEscRegister
(pHandle, 0x120, alEscCtrlStatus);
EC_API_SLV_writeByteEscRegister
uint32_t EC_API_SLV_writeByteEscRegister(EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint8_t value)
Write to virtual ESC register.
Definition
ecSlvApi.c:2054
Basic Functions
generated by
1.9.8