EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_readDoubleWordEscRegister()

uint32_t EC_API_SLV_readDoubleWordEscRegister ( EC_API_SLV_SHandle_t pHandle,
uint16_t  escAddress,
uint32_t *  pValue 
)

This is the function reads a byte from ESC Register.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]escAddressThe ESC Address
[out]pValueRegister value
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
uint32_t alEscCtrlStatus = 0;
// the Call
uint32_t error = EC_API_SLV_readDoubleWordEscRegister(pHandle, 0x120, &alEscCtrlStatus);
uint32_t EC_API_SLV_readDoubleWordEscRegister(EC_API_SLV_SHandle_t *pHandle, uint16_t escAddress, uint32_t *pValue)
This is the function reads a byte from ESC Register.
Definition ecSlvApi.c:2009
See also
EC_API_SLV_readByteEscRegister, EC_API_SLV_readWordEscRegister
Examples
ESL_cia402Demo.c.