EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_setStationAlias()

uint32_t EC_API_SLV_setStationAlias ( EC_API_SLV_SHandle_t pHandle,
uint16_t  stationAlias 
)

This is the function to set station alias.

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]stationAliasNode station alias
Returns
ErrorCode API Error Code
Example
#include <ecSlvApi.h>
// required variables
EC_API_EError_t retVal = 0;
// the Call
retVal = EC_API_SLV_setStationAlias(pHandle, 1001);
uint32_t EC_API_SLV_setStationAlias(EC_API_SLV_SHandle_t *pHandle, uint16_t stationAlias)
This is the function to set station alias.
Definition ecSlvApi.c:1771
enum EC_API_EError EC_API_EError_t