EtherCAT SubDevice
 
Loading...
Searching...
No Matches

◆ EC_API_SLV_enableMdioManualMode()

uint32_t EC_API_SLV_enableMdioManualMode ( EC_API_SLV_SHandle_t pHandle,
uint32_t  manualMdioAddress,
uint32_t  firmwareConfig 
)

Enable mdio manual mode (TI workaround enable)

Parameters
[in]pHandleThe pointer to the EtherCAT API instance.
[in]manualMdioAddressmanual mdio mode address register
[in]firmwareConfigmanual mdio firmware mode config
Returns
error code
Example
#include <ecSlvApi.h>
// the Call
EC_API_SLV_enableMdioManualMode(pHandle, MDIO_MANUAL_MODE_BASE_ADDRESS, MDIO_MANUAL_MODE_FW_CONFIG_VALUE);
uint32_t EC_API_SLV_enableMdioManualMode(EC_API_SLV_SHandle_t *pHandle, uint32_t manualMdioAddress, uint32_t firmwareConfig)
Enable mdio manual mode (TI workaround enable)
Definition ecSlvApi.c:2256