| typedef bool(* EC_API_SLV_EoE_CBSettingIndHandler_t) (void *pContext, uint16_t *pMac, uint16_t *pIp, uint16_t *pSubNet, uint16_t *pDefaultGateway, uint16_t *pDnsIp) |
EoE Settings Indication callback proxy.
| [in] | pContext | The pointer to the EtherCAT API instance. |
| [in] | pMac | Virtual Net MAC address |
| [in] | pIp | Virtual Net IP address |
| [in] | pSubNet | Virtual Net Subnet |
| [in] | pDefaultGateway | Virtual Net Default Gateway |
| [in] | pDnsIp | Virtual Net DNS server address |