EtherCAT SubDevice
 
Loading...
Searching...
No Matches
EEPROM Configuration

The EtherCAT SubDevice information is generated on the fly and by default is not stored anywhere, it’s simply emulated. However, the SDK provides a set of functions to store the EtherCAT SubDevice information content in a physical storage. Therefore, after a hardware reset the SDK will use the content from the non-volatile memory instead of the content generated on the fly. For detailed implementation overview refer to the file, YOUR_SDK_VERSION_DIRECTORY\examples\industrial_comms\ethercat_subdevice_demo\common\os\freertos\ESL_eeprom.c

For more information on non-volatile memory interface, please refer the page Non-Volatile Memory (NVM).

Function Description
EC_API_SLV_EEPROM_cbRegisterInit Register non-volatile memory initialization function
EC_API_SLV_EEPROM_cbRegisterRead Register non-volatile memory read function
EC_API_SLV_EEPROM_cbRegisterWrite Register non-volatile memory write function