RAS/RAP For Channel Sounding

This chapter serves as a guide for understanding what the Ranging Service (RAS) and Ranging Profile (RAP) are, their purpose, and how they fit into the context of Channel Sounding (CS). It also provides an overview of the architecture defined by the ranging service and profile. The guide will discuss the implementation, and usage of the RAS/RAP client and server.

Why RAP/RAS

The RAP client is used to request data from the peer device generating CS data within a CS procedure. The peer device is a RAP server side.

RAS standardizes the transfer of CS data. It is used in applications such as car access, asset tracking, geo-fencing and more.

Note

According to the Ranging Profile specification, pairing must be enabled to use RRSP and RREQ, even to discover the features.

RAS/RAP Overview

RAS is a standardized method to collect and exchange of ranging data.

The RAP uses a client-server model to exchange CS data between the two devices. It contains two roles, which are used to exchange ranging results. The first is the Ranging Responder (RRSP) and corresponds with the server side. The second role is the Ranging Requester (RREQ) and corresponds with the client side.

The RREQ initiates characteristic discovery for a device with server capabilities, and requests data from the RRSP. It must be able to enable RAS characteristics host by RRSP side.

The RRSP is the device that is the GATT Server. The RRSP hosts the RAS and stores ranging data for future transmission. It will send its capabilities to the RREQ after a request and transfer results according to the method they both support and choose.

Note

The RRSP and RREQ roles are independent of gap roles (central/peripheral) and CS roles (initiator/reflector).

RAS/RAP Client Architecture

The below image outlines the architecture of RAS/RAP.

../_images/ditaa-d631adb4c50bb37b5c32eee5e5978668371d72c2.png

The RAS is utilized by the device assigned to the RRSP role , which is responsible for generating the ranging results. The RAS supports two modes of data exchange:

  • Real-time Ranging Data: Instantly transmits the collected ranging data to the RREQ.

  • On-Demand Ranging Data: Saves the ranging data on the RAS server for later retrieval by the RREQ.

The RRSP dictates the data exchange mode. The RRSQ will enable notifications or indications which communicate the mode of data exchange. If the RRSP enables Real-time Ranging Data notifications or indications, the RREQ will configure to receive the data segments in real time. The RRSP will begin to send CS procedure data to the RREQ immediately after the CS procedure is completed. If the RRSP enables On-Demand Ranging Data notifications or indications, then the RRSP will save the data for later retrieval. When the RREQ is ready to receive the ranging data, the RREQ will send a Get Ranging Data command to the RRSP. The RRSP will then begin to send the CS procedure data to the RREQ using on demand ranging data notifications of indications. Additionally, if one or more segments of data is not received by the RREQ, the RREQ write a Request Lost Ranging Data command. The command will request will specify the missing data segments and trigger the RRSP to resend the segments. The RRSP will respond with the mode notification or indication, then send the lost ranging data to the RREQ. If the RRSP has already written over the lost data, the RRSP will respond with a No Records Found command. The RREQ must send a Acknowledgement of Ranging Data command or a Retrieve Lost Ranging Data command before the configured timeout. The maximum timeout is 10 seconds.

The RAS operates in only one mode at a time, determined by the user configuration. Examples of both modes are provided below:

@startuml

participant Client
participant "RAS Server"

rnote over "RAS Server"
    CS Subevent Results Info (Ranging Counter 0 with 6 subevents)
end note

group "Real-time Ranging Data"

  "RAS Server" -> Client  : Real-time Rangign Data notification or indication (1st segment)
  "RAS Server" -> Client  : Real-time Rangign Data notification or indication (nth segment)
  "RAS Server" -> Client  : Real-time Rangign Data notification or indication (last segment)

end group

rnote over "RAS Server"
   CS Subevent Results Info (Ranging Counter 1 with 6 subevents)
end note

group Real-time Ranging Data

  "RAS Server" -> Client  : Real-time Rangign Data notification or indication (1st segment)
  "RAS Server" -> Client  : Real-time Rangign Data notification or indication (nth segment)
  "RAS Server" -> Client  : Real-time Rangign Data notification or indication (last segment)

end group

rnote over "RAS Server"
    CS Subevent Results Info (Ranging Counter 1 with 6 subevents)
end note

@enduml

RAS Real-Time Ranging Data Exchange

@startuml


participant Client
participant "RAS Server"

rnote over "RAS Server"
    CS Subevent Results Info (Ranging Counter 0 with 6 subevents)
end note

group On-Demande Ranging Data exchange procedure

    "RAS Server" -> Client  : Ranging Data Ready indication (Ranging Counter = 0)
    Client -> "RAS Server"  : Get_Ranging Data command (Op Code: 0x00, Parameter #1: Ranging Counter = 0)

    group On-Demand Ranging Data
        "RAS Server" -> Client  : On-Demand Ranging Data notification or indication ((1st segment) = 0)
        "RAS Server" -> Client  : On-Demand Ranging Data notification or indication (nth segment)
        "RAS Server" -> Client  : On-Demand Ranging Data notification or indication (last segment)
    end group

    "RAS Server" -> Client  : Complete Ranging Data repsonse (Op Code: 0x00, Parameter #1: Ranging Counter = 0)
     Client -> "RAS Server"  : ACK_Ranging Data command (Op Code: 0x01, Parameter #1: Ranging Counter = 0)
    "RAS Server" -> Client  : Response Code (Op Code: 0x02, Parameter #1: 0x01 Success)

end group

rnote over "RAS Server"
    CS Subevent Results Info (Ranging Counter 1 with 5 subevents)
end note

@enduml

RAS On Demand Ranging Data Exchange

The RREQ supports an abort operation command. The abort operation is used for on demand ranging data indications or notifications. If the RREQ does not receive an on demand ranging data indication or notification within 5 seconds of sending an Get Ranging Data command, then the operation will abort. The RREQ will then write an abort command to the RRSP. Additionally, if the RREQ does not receive an on demand indication or notification 1 second after the previous on demand indication or notification, then the RREQ will send an abort command.

RRSP Ranging Data Packet structure

The ranging data sent by the RAS server via the RRSP role, is standardized. The packet begins with a Ranging Header. The Ranging Header contains the following fields:

  • ACL Connection Event: The ACL connection event after the previous CS event is completed, which will be the transmission of CS payload.

  • Frequency Compensation: 15-bit signed integer value that represents the frequency compensation in parts per million (ppm).

  • Ranging Done Status: Indicates the status of the CS procedure.

  • Subevent Done Status: Indicates the status of the CS subevent.

  • Ranging Abort Reason: Communicates the CS procedure abort reason.

  • Subevent Abort Reason: Communicates the CS subevent abort reason.

  • Reference Power Level: Represents the reference power level from -127 to 20 dBm.

  • Number of Steps Reported: Number of steps within the CS subevent that the RRSP is reporting.

The Ranging Header is sent by the RRSP at the beginning of the data transmission. After, a Subevent Header is sent before each subevents worth of data is reported. The Subevent Header contains the following fields:

  • Step Mode [i]: Amount of steps reported by the RRSP multiplied by 8.

  • Step Data [i]: Data specific to each step. Represents information about the mode and role of the steps being reported.

The structure of RRSP reporting packets is defined by RAS and is described in the image below:

../_images/RangingBody.png

Ranging Data Segment