SimpleLink Common Components Module 9.14.01 Release Notes

Table of Contents

Introduction

The SimpleLink Common Components Module (SCCM) includes NV Interface (Non-volatile Memory Interface) and MCUboot. These release notes include bug fixes, updates, and new features for the SCCM components.

Documentation

The follow table details which SCCM components are supported by the different SimpleLink stacks

Stack NV MCUboot
BLE X X
PropRF X
Zigbee X X

What’s New

ID Summary
SCCM-592 CC27XX HSM BareMetal module shall support Asymmetric Asset operations
SCCM-591 CC27XX HSM BareMetal Module shall support one key blob element

Fixed Issues

ID Summary
SCCM-621 Extra trailer length of 0x630 getting introduced

Known Issues and Limitations

ID Summary
None None

It should be noted that multiple external NVS regions are not supported. If a user attempts to create a second external NVS region, all actions on the second region will be done on the first region.

Upgrade and Compatibility Information

Dependencies

SCCM components were built & tested with the Integrated Development Environments (IDEs) and listed in the top-level SDK release notes.

Technical Support and Product Updates