API Documentation  9.14.02
Data Fields
UART2_Config_ Struct Reference

UART2 Global configuration. More...

Data Fields

void const * hwAttrs
 
void * object
 

Detailed Description

UART2 Global configuration.

The UART2_Config structure contains a set of pointers used to characterize the UART2 driver implementation.

Field Documentation

§ hwAttrs

void const* UART2_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure

§ object

void* UART2_Config_::object

Pointer to a driver specific data object


The documentation for this struct was generated from the following file: