API Documentation  9.14.02
Data Fields
Power_NotifyObj Struct Reference

Power notify object structure. More...

Data Fields

uintptr_t clientArg
 
uint_fast16_t eventTypes
 
List_Elem link
 
Power_NotifyFxn notifyFxn
 

Detailed Description

Power notify object structure.

This structure specification is for internal use. Notification clients must pre-allocate a notify object when registering for a notification; Power_registerNotify() will take care initializing the internal elements appropriately.

See also
Using power notify

Field Documentation

§ clientArg

uintptr_t Power_NotifyObj::clientArg

argument provided by client

§ eventTypes

uint_fast16_t Power_NotifyObj::eventTypes

the event type

§ link

List_Elem Power_NotifyObj::link

for placing on the notify list

§ notifyFxn

Power_NotifyFxn Power_NotifyObj::notifyFxn

notification function


The documentation for this struct was generated from the following file: