API Documentation  9.14.02
Data Fields
PDMCC26XX_metaData Struct Reference

Metadata associated with an array of PCM data. More...

Data Fields

int16_t pv
 
uint8_t seqNum
 
int8_t si
 

Detailed Description

Metadata associated with an array of PCM data.

Field Documentation

§ pv

int16_t PDMCC26XX_metaData::pv

Next predicted value of a PDMCC26XX_pcmBuffer

§ seqNum

uint8_t PDMCC26XX_metaData::seqNum

Sequence number of a PDMCC26XX_pcmBuffer

§ si

int8_t PDMCC26XX_metaData::si

Step index of a PDMCC26XX_pcmBuffer


The documentation for this struct was generated from the following file: