API Documentation  9.14.02
Data Fields
I2C_Config_ Struct Reference

I2C driver's custom configuration structure. More...

Data Fields

void const * hwAttrs
 
void * object
 

Detailed Description

I2C driver's custom configuration structure.

See also
I2C_init()
I2C_open()

Field Documentation

§ hwAttrs

void const* I2C_Config_::hwAttrs

Pointer to a driver specific hardware attributes structure.

§ object

void* I2C_Config_::object

Pointer to a driver specific data object.


The documentation for this struct was generated from the following file: