API Documentation  9.14.02
Data Structures | Macros | Typedefs | Enumerations | Functions | Variables
UART2.h File Reference

PRELIMINARY UART driver interface More...

Go to the source code of this file.

Data Structures

struct  UART2_Config_
 UART2 Global configuration. More...
 
struct  UART2_Params
 UART2 Parameters. More...
 

Macros

#define UART2_EVENT_BREAK   (0x04)
 A break has occurred.
 
#define UART2_EVENT_FRAMING   (0x01)
 A framing error has occurred.
 
#define UART2_EVENT_OVERRUN   (0x08)
 A receive overrun has occurred.
 
#define UART2_EVENT_PARITY   (0x02)
 A parity error has occurred.
 
#define UART2_EVENT_TX_BEGIN   (0x10)
 The UART will start transmitting data. More...
 
#define UART2_EVENT_TX_FINISHED   (0x20)
 The UART stopped transmitting data. More...
 
#define UART2_FLOWCTRL_HARDWARE   1
 Hardware flow control.
 
#define UART2_FLOWCTRL_NONE   0
 No hardware flow control.
 
#define UART2_STATUS_EAGAIN   (-16)
 A UART2_write() or UART2_read() in UART2_Mode_NONBLOCKING would have blocked.
 
#define UART2_STATUS_EBREAK   (-4)
 A break error occurred.
 
#define UART2_STATUS_ECANCELLED   (-14)
 A UART2_write() or UART2_read() operation was cancelled.
 
#define UART2_STATUS_EFAIL   (-11)
 General failure status returned by UART2 API.
 
#define UART2_STATUS_EFRAMING   (-1)
 A framing error occurred.
 
#define UART2_STATUS_EINUSE   (-9)
 The UART is currently in use.
 
#define UART2_STATUS_EINVALID   (-10)
 An invalid argument or UART2_Params field was passed to UART2 API.
 
#define UART2_STATUS_EMEMORY   (-12)
 A memory allocation failure occurred.
 
#define UART2_STATUS_ENOTOPEN   (-15)
 A UART2_write() or UART2_read() called on a device not opened.
 
#define UART2_STATUS_EOVERRUN   (-8)
 A FIFO overrun occurred.
 
#define UART2_STATUS_EPARITY   (-2)
 A parity error occurred.
 
#define UART2_STATUS_ETIMEOUT   (-13)
 A timeout occurred for a blocking UART2_read or UART2_write call.
 
#define UART2_STATUS_SREADTIMEOUT   (1)
 A read timeout occurred (not an error).
 
#define UART2_STATUS_SUCCESS   (0)
 Successful status code returned by UART2 APIs.
 
#define UART2_WAIT_FOREVER   (~(0U))
 Wait forever define.
 

Typedefs

typedef void(* UART2_Callback) (UART2_Handle handle, void *buf, size_t count, void *userArg, int_fast16_t status)
 The definition of a callback function used by the UART2 driver when used in UART2_Mode_CALLBACK The callback can occur in task or interrupt context. More...
 
typedef struct UART2_Config_ UART2_Config
 UART2 Global configuration. More...
 
typedef void(* UART2_EventCallback) (UART2_Handle handle, uint32_t event, uint32_t data, void *userArg)
 The definition of a callback function used by the UART driver. The callback can occur in task or interrupt context. More...
 
typedef struct UART2_Config_UART2_Handle
 A handle that is returned from a UART2_open() call.
 

Enumerations

enum  UART2_DataLen { UART2_DataLen_5 = 0, UART2_DataLen_6 = 1, UART2_DataLen_7 = 2, UART2_DataLen_8 = 3 }
 UART2 data length settings. More...
 
enum  UART2_Mode { UART2_Mode_BLOCKING, UART2_Mode_CALLBACK, UART2_Mode_NONBLOCKING }
 UART2 mode settings. More...
 
enum  UART2_Parity {
  UART2_Parity_NONE = 0, UART2_Parity_EVEN = 1, UART2_Parity_ODD = 2, UART2_Parity_ZERO = 3,
  UART2_Parity_ONE = 4
}
 UART2 parity type settings. More...
 
enum  UART2_ReadReturnMode { UART2_ReadReturnMode_FULL, UART2_ReadReturnMode_PARTIAL }
 UART2 return mode settings. More...
 
enum  UART2_StopBits { UART2_StopBits_1 = 0, UART2_StopBits_2 = 1 }
 UART2 stop bit settings. More...
 

Functions

void UART2_close (UART2_Handle handle)
 Function to close a UART peripheral specified by the UART2 handle. More...
 
void UART2_flushRx (UART2_Handle handle)
 Function to flush data in the UART RX FIFO. More...
 
size_t UART2_getRxCount (UART2_Handle handle)
 Get the number of bytes available in the circular buffer. More...
 
UART2_Handle UART2_open (uint_least8_t index, UART2_Params *params)
 Function to initialize a given UART peripheral. More...
 
void UART2_Params_init (UART2_Params *params)
 Function to initialize the UART2_Params struct to its defaults. More...
 
int_fast16_t UART2_read (UART2_Handle handle, void *buffer, size_t size, size_t *bytesRead)
 Function that reads data from a UART. More...
 
void UART2_readCancel (UART2_Handle handle)
 Function that cancels a UART2_read() function call. More...
 
int_fast16_t UART2_readTimeout (UART2_Handle handle, void *buffer, size_t size, size_t *bytesRead, uint32_t timeout)
 Function that reads data from a UART, with a specified timeout for blocking mode. More...
 
void UART2_rxDisable (UART2_Handle handle)
 Function that disables collecting of RX data into the circular buffer. More...
 
void UART2_rxEnable (UART2_Handle handle)
 Function that enables collecting of RX data into the circular buffer. More...
 
int_fast16_t UART2_write (UART2_Handle handle, const void *buffer, size_t size, size_t *bytesWritten)
 Function that writes data to a UART. More...
 
void UART2_writeCancel (UART2_Handle handle)
 Function that cancels a UART2_write() function call. More...
 
int_fast16_t UART2_writeTimeout (UART2_Handle handle, const void *buffer, size_t size, size_t *bytesWritten, uint32_t timeout)
 Function that writes data to a UART, with a specified timeout. More...
 

Variables

const UART2_Config UART2_config []
 
const uint_least8_t UART2_count
 

Detailed Description

PRELIMINARY UART driver interface


WARNING These APIs are PRELIMINARY, and subject to change in the next few months.

The UART2 driver is an updated version of the UART driver. The name UART2 was given due to changes in the API, to support backwards compatibility with applications using the existing UART driver. Key differences between the UART and UART2 drivers:

This module serves as the main interface for applications. Its purpose is to implement common code between the device specific implementations of UART2. Any device specific code that differs from the common code is called through functions prefaced with the "UART2_" naming convention. These functions are implemented in each device specific implementation.

Overview

A UART is used to translate data between the chip and a serial port. The UART2 driver simplifies reading and writing to any of the UART peripherals on the board, with multiple modes of operation and performance. These include blocking and nonblocking modes.

The UART2 driver interface provides device independent APIs, data types, and macros. The APIs in this driver serve as an interface to a typical RTOS application. The specific peripheral implementations are responsible for creating all the RTOS specific primitives to allow for thread-safe operation.


Usage

This documentation provides a basic usage summary and a set of examples in the form of commented code fragments. Detailed descriptions of the APIs are provided in subsequent sections.

Synopsis

// Import the UART2 driver definitions
// Initialize UART2 parameters
UART2_Params params;
params.baudRate = 9600;
// Open the UART
uart = UART2_open(CONFIG_UART0, &params);
// Enable receiver, inhibit low power mode
// Read from the UART.
size_t bytesRead;
uint8_t buffer[BUFSIZE];
int32_t status;
status = UART2_read(uart, buffer, BUFSIZE, &bytesRead);
// Write to the UART
size_t bytesWritten;
status = UART2_write(uart, buffer, BUFSIZE, &bytesWritten);
// Close the UART

Examples

The following code example opens a UART instance, reads a byte from the UART, and then writes the byte back to the UART.

char input;
UART2_Params uartParams;
// Open an instance of the UART2 driver
UART2_Params_init(&uartParams);
uartParams.baudRate = 115200;
uart = UART2_open(CONFIG_UART0, &uartParams);
if (uart == NULL) {
// UART2_open() failed
while (1);
}
// Enable receiver, inhibit low power mode
// Loop forever echoing
while (1) {
status = UART2_read(uart, &input, 1, &bytesRead);
status = UART2_write(uart, &input, 1, &bytesWritten);
}

Details for the example code above are described in the following subsections.

Opening the UART2 Driver

Opening a UART requires four steps:

  1. Create and initialize a UART2_Params structure.
  2. Fill in the desired parameters.
  3. Call UART2_open(), passing the index of the UART in the UART2_config structure, and the address of the UART2_Params structure. The UART2 instance is specified by the index in the UART2_config structure.
  4. Check that the UART2 handle returned by UART2_open() is non-NULL, and save it. The handle will be used to read and write to the UART you just opened.

Only one UART index can be used at a time; calling UART2_open() a second time with the same index previously passed to UART2_open() will result in an error. You can, though, re-use the index if the instance is closed via UART2_close(). In the previous example code, CONFIG_UART0 is passed to UART2_open(). This macro is defined in the example's ti_drivers_config.h file.

Modes of Operation

The UART driver can operate in blocking, nonblocking, or callback mode, by setting the writeMode and readMode parameters passed to UART2_open(). If these parameters are not set, as in the example code, the UART2 driver defaults to blocking mode. Options for the writeMode and readMode parameters are UART2_Mode_BLOCKING, UART2_Mode_NONBLOCKING, and UART2_Mode_CALLBACK:

The example code enables the collection of data into the RX ring buffer before the first call to UART2_read():

Note that this call is not necessary if the first UART2_read() is called in time to prevent the RX FIFO from overrun, or if flow control is used.

Reading and Writing Data

The example code reads one byte from the UART instance, and then writes one byte back to the same instance:

status = UART2_read(uart, &input, 1, &bytesRead);
status = UART2_write(uart, &input, 1, &bytesWritten);

The UART2 driver allows full duplex data transfers. Therefore, it is possible to call UART2_read() and UART2_write() at the same time. It is not possible, however, to issue multiple concurrent operations in the same direction. For example, if one thread calls UART2_read(uart0, buffer0...), any other thread attempting UART2_read(uart0, buffer1...) will result in an error of UART2_STATUS_EINUSE, until all the data from the first UART2_read() has been transferred to buffer0. This applies to blocking, callback, and nonblocking modes. So applications must either synchronize UART2_read() (or UART2_write()) calls that use the same UART handle, or check for the UART2_STATUS_EINUSE return code indicating that a transfer is still ongoing.


Configuration

Refer to the Driver's Configuration section for driver configuration information.



Typedef Documentation

§ UART2_Callback

typedef void(* UART2_Callback) (UART2_Handle handle, void *buf, size_t count, void *userArg, int_fast16_t status)

The definition of a callback function used by the UART2 driver when used in UART2_Mode_CALLBACK The callback can occur in task or interrupt context.

Parameters
[in]UART2_HandleUART2_Handle
[in]bufPointer to read/write buffer
[in]countNumber of elements read/written
[in]userArgA user supplied argument specified in UART2_Params.
[in]statusA UART2_STATUS code indicating success or failure of the transfer.

§ UART2_Config

typedef struct UART2_Config_ UART2_Config

UART2 Global configuration.

The UART2_Config structure contains a set of pointers used to characterize the UART2 driver implementation.

§ UART2_EventCallback

typedef void(* UART2_EventCallback) (UART2_Handle handle, uint32_t event, uint32_t data, void *userArg)

The definition of a callback function used by the UART driver. The callback can occur in task or interrupt context.

Parameters
[in]UART2_HandleUART2_Handle
[in]eventUART2_EVENT that has occurred.
[in]data- UART2_EVENT_OVERRUN: accumulated count
  • UART2_EVENT_BREAK: unused
  • UART2_EVENT_PARITY: unused
  • UART2_EVENT_FRAMING: unused
  • UART2_EVENT_TX_BEGIN: unused
  • UART2_EVENT_TX_FINISHED: unused
[in]userArgA user supplied argument specified in UART2_Params.
[in]statusA UART2_STATUS code indicating success or failure of the transfer.

Enumeration Type Documentation

§ UART2_DataLen

UART2 data length settings.

This enumeration defines the UART data lengths.

Enumerator
UART2_DataLen_5 

Data length is 5 bits

UART2_DataLen_6 

Data length is 6 bits

UART2_DataLen_7 

Data length is 7 bits

UART2_DataLen_8 

Data length is 8 bits

§ UART2_Mode

enum UART2_Mode

UART2 mode settings.

This enum defines the read and write modes for the configured UART.

Enumerator
UART2_Mode_BLOCKING 

UART2_write() will block the calling task until all of the data has been transmitted onto the TX pin. UART2_read() will block until some data becomes available.

UART2_Mode_CALLBACK 

Nonblocking, UART2_write() or UART2_read() will return immediately. When all data has been either written to, or read from the hardware FIFO, the callback function is called from either the caller's context or from an interrupt context, and the driver is ready to accept a new call to UART2_write() or UART2_read(). It is not guaranteed that all data has been fully transmitted yet when the write-callback is invoked. To be notified of this, the application must subscribe to the UART2_EVENT_TX_FINISHED event.

UART2_Mode_NONBLOCKING 

Nonblocking, UART2_write() or UART2_read() will return immediately. UART2_write() will copy as much data into the transmit buffer as space allows. UART2_read() will copy as much data from the receive buffer as is immediately available.

§ UART2_Parity

UART2 parity type settings.

This enumeration defines the UART2 parity types.

Enumerator
UART2_Parity_NONE 

No parity

UART2_Parity_EVEN 

Parity bit is even

UART2_Parity_ODD 

Parity bit is odd

UART2_Parity_ZERO 

Parity bit is always zero

UART2_Parity_ONE 

Parity bit is always one

§ UART2_ReadReturnMode

UART2 return mode settings.

This enumeration defines the return modes for UART2_read().

UART2_ReadReturnMode_FULL unblocks or performs a callback when the read buffer has been filled with the number of bytes passed to UART2_read(). UART2_ReadReturnMode_PARTIAL unblocks or performs a callback whenever a read timeout error occurs on the UART peripheral. This timeout error is not the same as the blocking read timeout in the UART2_Params; the read timeout occurs if the read FIFO is non-empty and no new data has been received for a device/baudrate dependent number of clock cycles. This mode can be used when the exact number of bytes to be read is not known.

Enumerator
UART2_ReadReturnMode_FULL 

Unblock/callback when buffer is full.

UART2_ReadReturnMode_PARTIAL 

Unblock/callback when no new data comes in.

§ UART2_StopBits

UART2 stop bit settings.

This enumeration defines the UART2 stop bits.

Enumerator
UART2_StopBits_1 

One stop bit

UART2_StopBits_2 

Two stop bits

Function Documentation

§ UART2_close()

void UART2_close ( UART2_Handle  handle)

Function to close a UART peripheral specified by the UART2 handle.

Precondition
UART2_open() has been called.
There are no ongoing read or write calls. Any ongoing read or write calls can be cancelled with UART2_readCancel() or UART2_writeCancel().
Parameters
[in]handleA UART2_Handle returned from UART2_open()
See also
UART2_open()

§ UART2_flushRx()

void UART2_flushRx ( UART2_Handle  handle)

Function to flush data in the UART RX FIFO.

Precondition
UART2_open() has been called.

This function can be called to remove all data from the RX FIFO, for example, after a UART read error has occurred. All data in the RX circular buffer will be discarded.

Parameters
[in]handleA UART2_Handle returned from UART2_open()

§ UART2_getRxCount()

size_t UART2_getRxCount ( UART2_Handle  handle)

Get the number of bytes available in the circular buffer.

Precondition
UART2_open() has been called.
Parameters
[in]handleA UART2_Handle returned from UART2_open()
Returns
Returns the number of bytes available in the RX circular buffer.
See also
UART2_rxEnable()

§ UART2_open()

UART2_Handle UART2_open ( uint_least8_t  index,
UART2_Params params 
)

Function to initialize a given UART peripheral.

Function to initialize a given UART peripheral specified by the particular index value.

Parameters
[in]indexLogical peripheral number for the UART indexed into the UART2_config table
[in]paramsPointer to a parameter block. If NULL, default parameter values will be used. All the fields in this structure are read-only.
See also
UART2_close()

§ UART2_Params_init()

void UART2_Params_init ( UART2_Params params)

Function to initialize the UART2_Params struct to its defaults.

Parameters
[in]paramsA pointer to UART2_Params structure for initialization

Defaults values are: readMode = UART2_Mode_BLOCKING; writeMode = UART2_Mode_BLOCKING; eventCallback = NULL; eventMask = 0; readCallback = NULL; writeCallback = NULL; readReturnMode = UART2_ReadReturnMode_PARTIAL; baudRate = 115200; dataLength = UART2_DataLen_8; stopBits = UART2_StopBits_1; parityType = UART2_Parity_NONE; userArg = NULL;

§ UART2_read()

int_fast16_t UART2_read ( UART2_Handle  handle,
void *  buffer,
size_t  size,
size_t *  bytesRead 
)

Function that reads data from a UART.

UART2_read() reads data from a UART controller. The destination is specified by buffer and the number of bytes to read is given by size.

In UART2_Mode_BLOCKING, UART2_read() blocks task execution until all the data in buffer has been read, if the read return mode is UART2_ReadReturnMode_FULL. If the read return mode is UART2_ReadReturnMode_PARTIAL, UART2_read() returns before all the data has been read, if some data has been received, but reception has been inactive sufficiently long for a hardware read timeout to occur (e.g., for a 32-bit period). If a receive error occurs (e.g., framing, FIFO overrun), UART2_read() will return with the number of bytes read up to the occurance of the error.

In UART2_Mode_CALLBACK, UART2_read() does not block task execution. Instead, a callback function specified by UART2_Params::readCallback is called when the transfer is finished (UART2_ReadReturnMode_FULL), or reception has become inactive (UART2_ReadReturnMode_PARTIAL). The callback function can occur in the caller's context or in HWI context, depending on the device-specific implementation. An unfinished asynchronous read operation must always be cancelled using UART2_readCancel() before calling UART2_close().

In UART2_Mode_NONBLOCKING, UART2_read() will return the minimum of size bytes and the number of bytes in the RX circular buffer. In this mode, the application should check the number of bytes returned in the bytesRead parameter. A status of success will be returned, even if not all bytes requested were read, unless no data is available or an error occured. If no data is available, a status of UART2_STATUS_EAGAIN is returned.

Note
It is ok to call UART2_read() from its own callback function when in UART2_Mode_CALLBACK.
Warning
By calling this function, RX will be enabled even after the function has returned. This is in order to keep collecting data into the RX buffer to prevent losing data at high baud-rates. As a consequence, entering low power mode will be inhibited. To disable RX and enable entering low power mode, UART2_rxDisable must be called.
Parameters
[in]handleA UART2_Handle returned by UART2_open()
[in]bufferA pointer to an empty buffer to which received data should be read
[in]sizeThe number of bytes to be read into buffer
[out]bytesReadIf non-NULL, the location to store the number of bytes actually read into the buffer. If NULL, this parameter will be ignored. In callback mode, NULL could be passed in for this parameter, since the callback function will be passed the number of bytes read. In blocking mode, NULL can be passed, however, status should be checked in case the number of bytes requested was not received due to errors. In nonblocking mode, it is not recommended to pass NULL for this parameter, as it would be impossible to determine the number of bytes actually read.
Returns
Returns a status indicating success or failure of the read.
Return values
UART2_STATUS_SUCCESSThe call was successful.
UART2_STATUS_EINUSEAnother read from the UART is currently ongoing.
UART2_STATUS_EAGAINIn UART2_Mode_NONBLOCKING, no data is currently available.
UART2_STATUS_ECANCELLEDIn UART2_Mode_BLOCKING, the read was canceled by a call to UART2_readCancel() before any data could be received.

§ UART2_readCancel()

void UART2_readCancel ( UART2_Handle  handle)

Function that cancels a UART2_read() function call.

This function cancels an asynchronous UART2_read() operation in in UART2_Mode_CALLBACK, or unblocks a UART2_read() call in UART2_Mode_BLOCKING. In UART2_Mode_CALLBACK, UART2_readCancel() calls the registered read callback function with the number of bytes received so far. It is the application's responsibility to check the count argument in the callback function and handle the case where only a subset of the bytes were received. The callback function will be passed a status of UART2_STATUS_ECANCELLED.

In UART2_Mode_BLOCKING, UART2_read() will return UART2_STATUS_ECANCELLED, and the bytesRead parameter will be set to the number of bytes received so far.

This API has no affect in UART2_Mode_NONBLOCKING.

Parameters
[in]handleA UART2_Handle returned by UART2_open()

§ UART2_readTimeout()

int_fast16_t UART2_readTimeout ( UART2_Handle  handle,
void *  buffer,
size_t  size,
size_t *  bytesRead,
uint32_t  timeout 
)

Function that reads data from a UART, with a specified timeout for blocking mode.

UART2_readTimeout() reads data from a UART controller. The destination is specified by buffer and the number of bytes to read is given by size.

In UART2_Mode_BLOCKING with UART2_ReadReturnMode_FULL, UART2_readTimeout() blocks task execution until all the data in buffer has been read, or the specified timeout has elapsed. In UART2_Mode_BLOCKING with UART2_ReadReturnMode_PARTIAL, UART2_readTimeout() returns before all the data has been read, if some data has been received, but reception has been inactive sufficiently long for a hardware read timeout to occur (e.g., for a 32-bit period). UART2_readTimeout() will also return if the specified timeout parameter has elapsed. Note that the timeout parameter is different from the hardware read timeout.

In UART2_Mode_CALLBACK, UART2_readTimeout() does not block task execution. Instead, a callback function specified by UART2_Params::readCallback is called when the transfer is finished (UART2_ReadReturnMode_FULL), or reception has become inactive (UART2_ReadReturnMode_PARTIAL). The callback function can occur in the caller's context or in HWI context, depending on the device-specific implementation. An unfinished asynchronous read operation must always be cancelled using UART2_readCancel() before calling UART2_close(). In UART2_Mode_CALLBACK, the timeout parameter passed to UART2_readTimeout(), is ignored.

In UART2_Mode_NONBLOCKING, UART2_readTimeout() will return the minimum of size and the number of data in the RX circular buffer. In this mode, the application should check the number of bytes read in the bytesRead parameter. A status of success will be returned if one or more bytes is available, unless an error occured. In UART2_Mode_NONBLOCKING, the timeout parameter passed to UART2_readTimeout(), is ignored.

Note
It is ok to call UART2_readTimeout() from its own callback function when in UART2_Mode_CALLBACK.
Warning
By calling this function, RX will be enabled even after the function has returned. This is in order to keep collecting data into the RX buffer to prevent losing data at high baud-rates. As a consequence, entering low power mode will be inhibited. To disable RX and enable entering low power mode, UART2_rxDisable must be called.
Parameters
[in]handleA UART2_Handle returned by UART2_open()
[in]bufferA pointer to an empty buffer to which received data should be read
[in]sizeThe number of bytes to be read into buffer
[out]bytesReadIf non-NULL, the location to store the number of bytes actually read into the buffer. If NULL, this parameter will be ignored. In callback mode, NULL could be passed in for this parameter, since the callback function will be passed the number of bytes read. Similarly, in blocking mode with infinite timeout, NULL can be passed. However, status should be checked in case the number of bytes requested was not received due to errors. In nonblocking mode, it is not recommended to pass NULL for this parameter, as it would be impossible to determine the number of bytes actually read.
[in]timeoutThe number of system clock ticks to wait until all data is received. If not all requested data was received within the timeout period, an error of UART2_STATUS_ETIMEOUT will be returned. This parameter is only applicable to UART2_Mode_BLOCKING.
Returns
Returns a status indicating success or failure of the read.
Return values
UART2_STATUS_SUCCESSThe call was successful.
UART2_STATUS_EINUSEAnother read from the UART is currently ongoing.
UART2_STATUS_EAGAINIn UART2_Mode_NONBLOCKING, no data is currently available.
UART2_STATUS_ECANCELLEDIn UART2_Mode_BLOCKING, the read was canceled by a call to UART2_readCancel() before any data could be received.
UART2_STATUS_ETIMEOUTThe read operation timed out.

§ UART2_rxDisable()

void UART2_rxDisable ( UART2_Handle  handle)

Function that disables collecting of RX data into the circular buffer.

The driver implementation uses a circular buffer to collect RX data while a UART2_read() is not in progress. This function will disable buffering of RX data into the circular buffer. UART2_read() will read directly from the UART driver's RX buffer. Disabling the circular buffer will also allow the device to go into low power modes.

Parameters
[in]handleA UART2_Handle returned by UART2_open()
See also
UART2_rxEnable()

§ UART2_rxEnable()

void UART2_rxEnable ( UART2_Handle  handle)

Function that enables collecting of RX data into the circular buffer.

The driver implementation uses a circular buffer to collect RX data while a UART2_read() is not in progress. This function will enable buffering of RX data into the circular buffer. UART2_read() will read directly from the UART drivers RX buffer. Enabling the circular buffer will also prevent the device from going into low power modes.

Parameters
[in]handleA UART2_Handle returned by UART2_open()
See also
UART2_rxDisable()

§ UART2_write()

int_fast16_t UART2_write ( UART2_Handle  handle,
const void *  buffer,
size_t  size,
size_t *  bytesWritten 
)

Function that writes data to a UART.

UART2_write() writes data from a memory buffer to the UART interface. The source is specified by buffer and the number of bytes to write is given by size.

In UART2_Mode_BLOCKING, UART2_write() blocks task execution until all the data in buffer has been transmitted onto the TX pin.

In UART2_Mode_CALLBACK, UART2_write() does not block task execution. Instead, a callback function specified by UART2_Params::writeCallback is called when all data has been written to the hardware FIFO. This means that that driver is ready to accept another call to UART2_write().

Note
In contrast to UART2_Mode_BLOCKING, it is not guaranteed that all data has been transmitted onto the TX pin when callback is invoked. This is instead signalled by the event UART2_EVENT_TX_FINISHED.

The buffer passed to UART2_write() in UART2_Mode_CALLBACK is not copied. The buffer must remain coherent until all the characters have been sent (ie until the write callback has been called with a byte count equal to that passed to UART2_write()). The callback function can occur in the caller's task context or in interrupt context, depending on the device implementation. An unfinished asynchronous write operation must always be cancelled using UART2_writeCancel() before calling UART2_close().

In UART2_Mode_NONBLOCKING, UART2_write() will send out as many of the bytes in the buffer as possible, until the TX circular buffer is full. In nonblocking mode, UART2_write() can be called from any context. The bytesWritten parameter should not be NULL so the application can determine the number of bytes actually written.

Parameters
[in]handleA UART2_Handle returned by UART2_open()
[in]bufferA read-only pointer to buffer containing data to be written to the UART
[in]sizeThe number of bytes in the buffer that should be written to the UART
[out]bytesWrittenIf non-NULL, the location to store the number of bytes actually written to the UART in UART2_Mode_BLOCKING and UART2_Mode_NONBLOCKING. In UART2_Mode_CALLBACK, bytesWritten will be set to 0. If bytesWritten is NULL, this parameter will be ignored. In nonblocking mode, it is not recommended to pass NULL for bytesWritten, as the application would have no way to determine the number of bytes actually written. In nonblocking mode, a status of success will be returned even if not all the requested bytes could be written.
Returns
Returns a status indicating success or failure of the write.
Return values
UART2_STATUS_SUCCESSThe call was successful.
UART2_STATUS_EINUSEAnother write to the UART is currently ongoing.

§ UART2_writeCancel()

void UART2_writeCancel ( UART2_Handle  handle)

Function that cancels a UART2_write() function call.

This function cancels an asynchronous UART2_write() operation when write mode is UART2_Mode_CALLBACK, or an ongoing UART2_write() in UART2_Mode_NONBLOCKING. In callback mode, UART2_writeCancel() calls the registered write callback function no matter how many bytes were sent. It is the application's responsibility to check the count argument in the callback function and handle cases where only a subset of the bytes were sent. The callback function will be passed a status of UART2_STATUS_ECANCELLED. In blocking mode, UART2_write() will return UART2_STATUS_ECANCELLED.

Note
The above applies to UART2_writeTimeout() as well.

This API has no affect in nonblocking mode.

Parameters
[in]handleA UART2_Handle returned by UART2_open()

§ UART2_writeTimeout()

int_fast16_t UART2_writeTimeout ( UART2_Handle  handle,
const void *  buffer,
size_t  size,
size_t *  bytesWritten,
uint32_t  timeout 
)

Function that writes data to a UART, with a specified timeout.

UART2_writeTimeout() writes data from a memory buffer to the UART interface. The source is specified by buffer and the number of bytes to write is given by size. A timeout in system clock ticks specifies the maximum time to wait until all data is written (UART2_Mode_BLOCKING only).

In UART2_Mode_BLOCKING, UART2_writeTimeout() blocks task execution until all the data in buffer has been transmitted, or the timeout expires.

In UART2_Mode_CALLBACK, UART2_writeTimeout() does not block task execution. Instead, a callback function specified by UART2_Params::writeCallback is called when all data has been written to the hardware FIFO. This means that that driver is ready to accept another call to UART2_writeTimeout().

Note
In contrast to UART2_Mode_BLOCKING, it is not guaranteed that all data has been transmitted onto the TX pin when callback is invoked. This is instead signalled by the event UART2_EVENT_TX_FINISHED.

The buffer passed to UART2_writeTimeout() in UART2_Mode_CALLBACK is not copied. The buffer must remain coherent until all the characters have been sent (ie until the write callback has been called with a byte count equal to that passed to UART2_writeTimeout()). The callback function can occur in the caller's task context or in interrupt context, depending on the device implementation. An unfinished asynchronous write operation must always be cancelled using UART2_writeCancel() before calling UART2_close().

In UART2_Mode_NONBLOCKING, UART2_writeTimeout() will send out as many of the bytes in the buffer as possible, until the TX FIFO is full. In nonblocking mode, UART2_writeTimeout() is nonblocking and can be called from any context. The bytesWritten parameter should not be NULL so the application can determine the number of bytes actually written.

Parameters
[in]handleA UART2_Handle returned by UART2_open()
[in]bufferA read-only pointer to buffer containing data to be written to the UART
[in]sizeThe number of bytes in the buffer that should be written to the UART
[out]bytesWrittenIf non-NULL, the location to store the number of bytes actually written to the UART in UART2_Mode_BLOCKING and UART2_Mode_NONBLOCKING. In UART2_Mode_CALLBACK, bytesWritten will be set to 0. If bytesWritten is NULL, this parameter will be ignored. In nonblocking mode, it is not recommended to pass NULL for bytesWritten, as the application would have no way to determine the number of bytes actually written. In nonblocking mode, a status of success will be returned even if not all the requested bytes could be written.
[in]timeoutThe number of system clock ticks to wait for the write to complete (UART2_Mode_BLOCKING only). If the timeout expires before all bytes are written, a status of UART2_STATUS_ETIMEOUT will be returned.
Returns
Returns a status indicating success or failure of the write.
Return values
UART2_STATUS_SUCCESSThe call was successful.
UART2_STATUS_EINUSEAnother write to the UART is currently ongoing.
UART2_STATUS_ETIMEOUTThe write operation timed out.