TI OAD API Documentation  9.14.02
Data Fields
HSMBareMetal_AssetPairStruct Struct Reference

Struct containing the two asset IDs returned for usage in a symmetric operation. More...

Data Fields

uint32_t * decVrfyKeyAssetID
 
uint32_t * encGenKeyAssetID
 
uint32_t * privateKeyAssetID
 
uint32_t * publicKeyAssetID
 

Detailed Description

Struct containing the two asset IDs returned for usage in a symmetric operation.

For any given plaintext key material, there exists two asset IDs.


The documentation for this struct was generated from the following file: